STEVAL-CAM-M0I Pinout compatibility with Raspberry Pi CM4
Hi, we are using the STEVAL-CAM-M0I board to evaluate the 55G0 protomodule.
I have it connected to a raspberry pi CM4 IO breakout board, to the CAM1 CSI-2 interface.
There is a provided driver, etc for this from ST, but it appears the pinout is not 1:1. But most of the documentation shows the eval board connecting directly to a raspberry pi. So I am wondering where does the issue lie here? Is the RST controlled by the GPIO, or am I missing something about the compatibility?
It was attractive because we didn't need to make an interface board.
I see the Reset pin and the Cam GPIO pins are swapped, along with the data lines. Raspberry PI Pinout:

and the STEVAL-CAM-M0I pinout:

Thanks