STEVAL-EVK-U0I and planned 5 Mp VD5943 and VD1943 Image Sensors
Hi,
I was wondering if it's planned for the current STEVAL-EVK-U0I board to work with the 5 Mp VD5943 and VD1943 Image Sensors when they're launched in spring 2026 or if a new USB interface board is planned for evaluation of VD5943 and VD1943?
The page for the STEVAL-EVK-U0I
https://www.st.com/en/evaluation-tools/steval-evk-u0i.html
says "CAM-56G3, CAM-66GY, CAM-55G0, CAM-55G1" so I wasn't sure if it was planned to for it to support evaluation of the VD5943 and VD1943 as well.
Will