Skip to main content
Visitor II
October 24, 2024
Question

STSW-IMG031 linux driver for VL53L4CX hosted anywhere?

  • October 24, 2024
  • 1 reply
  • 637 views

Hi there,

We want to use the VL53L4CX ToF sensor and I want to build the out of tree kernel module for the STSW-IMG031 (here) via Yocto recipe. Are the sources hosted anywhere on Github or elsewhere so I can clone the repo directly via Yocto rather than having to download the sources and add it to a private Github?

I've seen this SVN link on one of the docs in the driver package but could not access it via subversion - has the repo moved?

http://codex.cro.st.com/svnroot/ewokp25/LinuxDriver/tags/l3cx_release_1.0.3/

 

svn checkout http://codex.cro.st.com/svnroot/ewokp25/LinuxDriver/tags/l3cx_release_1.0.3 
svn: E170013: Unable to connect to a repository at URL 'http://codex.cro.st.com/svnroot/ewokp25/LinuxDriver/tags/l3cx_release_1.0.3'
svn: E670002: Name or service not known

Thanks,

Joe

 

1 reply

Anne BIGOT
Technical Moderator
October 24, 2024

Hello

The svn repo mentionned above is an internal release and should not appear in there. 
We will clean it. 

Regarding git, the linux driver is not yet available under any GitHub. Sorry for that.

Regards

Anne

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'