STSW-IMG501 Programmed Frame Rate Doesn't Match Software Output
I am using the STSW-IMG501 software with the STEVAL-EVK-U0I1 evaluation kit and the STEVAL-56G3MAI1 evaluation board for the VD56G3 image sensor. I am trying to capture videos of my target application at high frame rates to assess the sensor properties, but I am unable to get the STSW-IMG501 to capture at frame rates equivalent to what is programmed in the VD56G3 image sensor.
A short description of applicable frame rate parameters:
- Line Length - 1236 (0x0300, 0xd4, 0x04)
- Pixel Clock - 160.8 MHz
- Line Time - 7.69 us (Line Length / Pixel Clock)
- Subsampling/Binning Factor - 1 (no subsampling or binning)
- Ystart - 442 (0x045a, 0xba, 0x01)
- Yend - 921 (0x045c, 0x99, 0x03)
- Frame Length Offset - 69
- Minimum Frame Length - 549 ((Yend - Ystart+1)/(subsampling factor) + frame length offset)
- Target Frame Rate - 200 Hz
- Programmed Frame Length - 650 (0x0458, 0x8a, 0x02)
- Target Frame Duration - 5 ms
- Target Exposure Duration - 3.5 ms
- Coarse Exposure - 455 (0x044e, 0xc7, 0x01)
In order to verify my configuration of the frame rate, I configured GPIO0 to be FSYNC_OUT (0x0467, 0x00). To control the 74LVC1T45GF translating transceiver on the STEVAL-56G3MAI1, I set GPIO1 to be GPIO_OUT, High (0x0468, 0x15). I then soldered a wire onto the 0 Ohm jumper R55 on STEVAL-EVK-U0I1 and was able to measure a pulse waveform with frequency 200 Hz, so I know for certain that the VD56G3 is programmed to run at 200 Hz and is running at 200 Hz.
However, when running STSW-IMG501, the "execution rate" field in the upper left corner of the UI only jumps around ~60 FPS. When counting on fingers in front of the video, I can verify that a capture image sequence runs at ~70 FPS.
I did some research into the camera controller microcontroller used on the STEVAL-EVK-U0I1 (Infineon CX3) and it should be able to support 2.4 Gbps. Using similar back of paper calculations as seen on the Infineon dev community boards, I should be able to reach ~180 fps using the CX3, but I am still not seeing close to those rates (https://community.infineon.com/t5/USB-superspeed-peripherals/CX3-MIPI-Configure-for-1600x1200-resolution/td-p/706304#.).
That is all to say, what is the maximum frame rate capable of recording images from the STSW-IMG501? Are we hard limited to the ~60 Hz range, or is there additional parameterization I can perform to get it higher? Can we assume a uniform frame delay between frames? How can we measure the frame rate of image sequences captured in the STSW-IMG501? Some additional documentation in this area would be greatly appreciated.