Skip to main content
JGarrettW
Associate II
June 28, 2023
Solved

Time of Flight

  • June 28, 2023
  • 2 replies
  • 5432 views

..

This topic has been closed for replies.
Best answer by Anne BIGOT

Hello
There are some problems with this approach. The VCSELs generate a lot of EMi. To avoid them, the sensors provide a bit of spread spectrum clock jitter. This keeps the relatively large, fast power on/off from screwing up all the chips around it by having one large EMI spike.

But it seems you want to use the VCSEL output of one chip and the RX of lots of chips.

To do this they all have to run in lock step. And the jitter would prevent this from working.

It might be that you can disable the EMI protection on the chip, but then you still have to find some way to keep them in lock step. 

And interesting idea, but financially untenable. 

Regards

Anne

 

2 replies

Anne BIGOT
Anne BIGOTBest answer
Technical Moderator
July 27, 2023

Hello
There are some problems with this approach. The VCSELs generate a lot of EMi. To avoid them, the sensors provide a bit of spread spectrum clock jitter. This keeps the relatively large, fast power on/off from screwing up all the chips around it by having one large EMI spike.

But it seems you want to use the VCSEL output of one chip and the RX of lots of chips.

To do this they all have to run in lock step. And the jitter would prevent this from working.

It might be that you can disable the EMI protection on the chip, but then you still have to find some way to keep them in lock step. 

And interesting idea, but financially untenable. 

Regards

Anne

 

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'
JGarrettW
JGarrettWAuthor
Associate II
August 17, 2023

Deleted

John E KVAM
ST Employee
September 1, 2023

Unfortuantely that is exactly want it means. This approach has advantages (to everyone but you). Our chips don't interfere with each other (very much) because they operate with slightly different timings. And they don't cause problems for all the other chips in the design. 

To do what you are proposing, I think all the chips have to run on the same clock, otherwise slight variations in phase are going to make a mess of the timings.

- john