VD55G0 Video mode
According to the UM2829 manual stating that it supports "SLAVE_I2C STREAMING on I²C pulses", I would like to ask whether this means that image data can be obtained via I2C like the VD55G1, or if it only refers to synchronization signals between image data, with image transmission being possible only through MIPI CSI. Additionally, is there any code for obtaining images via I2C, such as starting to read from which address?