Solved
vl53l0x sensor detection distance inquiry
- April 18, 2024
- 2 replies
- 1761 views
(A translator was used for this inquiry.)
Hi,
I am using the vl53l0x sensor.
I would like to inquire about the detection range of the sensor.
- What value do you get when the wall you want to measure the distance against is tilted? (Refer to image1)
What point distance do you get if the minimum length between the sensor and the wall is 100 mm and the maximum is 200 mm? - I know that the maximum measurement distance of the sensor is 2M.
I would like to know the range of the detectable area when the wall and the sensor are 2M away.
(Refer to image2)
Thank you.