VL53L1 Water level measurement incorrect values
Hello.
I’m utilizing the VL53L1 sensor to measure water level inside of a closed water bucket.
While using a 30cm tall white bucket half full, with the VL53L1 positioned at the top aiming down at the air-water interface, the sensor sometimes outputs incorrect distance values for long periods of time. During one test run, the sensor spent almost half an hour outputting distance values oscillating within a 1,5cm range around the real distance value, later stabilizing on the correct distance value. This kind of issue has happened multiple times already on similar tests.
Given the water level and surface is completely static, I was wondering whether there are any minimum range limitations, given I’m measuring distance to a liquid and also utilizing a small recipient. The only minimum distance information I was able to find on the sensor’s datasheet is its 4cm minimum guaranteed ranging system.
Thanks in advance.