VL53L1X address changing
Hello,
We ordered some VL53L1X and put them on our PCB. We ran into a problem at the moment of changing the address: we can give these sensors only two address options 0x52 (default) and 0x53 so that they work correctly, but at other addresses the sensor initialization procedure looks correct, and the sensor can be seen, but during the measurement it returns only 0 mm.
We are wondering if there is a possibility of defective modules that we ordered? Or do we need to find the problem somewhere else? (we do not think this is a code, because on one module of the Pololu board, changing the address works fine) .
Best regards,
Aliaksandra