VL53L1X Boot period specs (setup time from hardware standby to SW standby)
Hello,
I am developing a system using VL53L1X.
Occasionally, when the host microcomputer is asynchronously reset,
there is no response from the sensor after that.
I've never used the xshut terminal.
If communication with the sensor becomes impossible,
I'm thinking of using the xshut terminal to synchronize the host microcomputer and the sensor.
Please let me know the setup time required to start I2C communication after setting the xshut pin to high level.
From the topic below, I think 10ms is enough, but I would like some information as a specification.
Title:vl53l1x-xshut-pin
Best regards.