VL53L1X Calibration Effect
I am observing an unexpected reading issue.
I am using Calibration and I use a physical distance to Calibrate. However, an object right in front of the sensor (1-20mm'ish away) reads a value of 0 (zero). If I change the Calibration to physical distance + 20 (rough) I get a better measurement of the object when its in front -- I get in fact more of a measurement I would expect. However, I would need to calibrate at a distance greater than the physical distance -- which is not what I thought one is supposed to do?