VL53L1X detect wrong with black object
Hi,
I'm building a project that uses 20 VL53L1x sensors to detect any people or objects that go in the danger zone of a machine.
The sensor will detect any objects or people below 2 meters distance. We set up the sensor 30cm above the ground.
The measure configure of sensor :
- Timing Budget MicroSeconds: 30ms.
- Inter measurement period MilliSeconds: 70ms.
- Do not use the glass cover.
I tested the reliability of the sensor and the result like below:
- People with blue, white pants are reliably detected.
- People with black khaki can not be detected by the sensor.
- People with black jeans can not be detected by the sensor.
I tested indoor.
I try to calibration. And I success to calibration RefSPAD, but I fails Offset and Crosstalk. It return error.
I called function in API:
1.VL53L1_WaitDeviceBooted
2.VL53L1_DataInit
3.VL53L1_StaticInit
4.VL53L1_PerformRefSpadManagement
5.VL53L1_SetMeasurementTimingBudgetMicroSeconds // I setting 30000
6.VL53L1_SetInterMeasurementPeriodMilliSeconds // I setting 40
7.VL53L1_PerformOffsetSimpleCalibration //I setting 140mm
8.VL53L1_PerformSingleTargetXTalkCalibration //I setting 140mm
9.VL53L1_GetCalibrationData
Please help me to explain this issue. Do you have any advice for me to detect reliability for all objects with all colors and materials?