VL53L1X Internal state that cannot respond to the I2C communication start condition
Hello,
I am developing a system using VL53L1X.
Occasionally, when the host microcomputer is asynchronously reset,
there is no response from the sensor after that.
It can be detected that the sensor's SDA is stuck at Low. We can handle it.
The situation I am encountering is that the sensor's SDA line is high, but I2C communication is not possible.
Is there an internal state that ignores the start condition from the host microcomputer?
If so, please tell me the transition conditions to that internal state.
Best regards.