VL53L4CD - Calibration Procedure and Tools
Hello,
I'm working with VL53L4CD to have the distance between the board and some liquid. This distance could go from 20mm to 250mm.
We want to protect the board with a glass and then do a calibration, first Offset then Crosstalk. Into the user manual, I found that I need to do the offset calibration on a 17% reflective target at 100 mm and the crosstalk calibration on 17% reflective target at maximum ranging distance without under-ranging.
My questions are :
- Do we really need a 17% reflective material as target ?
- 100mm is mandatory for the offset calibration ?
- As our system goes from 20 to 250mm, is it possible to perform the Crosstalk calibration or do we need to take the board outside of our machine to be at the right distance ?
Thank you for your help,
Kind regards,