VL53L4CD Power consumption measurement
Hello Everyone,
I'm using the VL53L4CD with the STM32WL55JC1, The following is the Power Profile of the cycle:
1- XSHUT GPIO is normally pulled low.
2- XSHUT Pulled up + delay ( sensor wakes up).
3- VL53L4CD Initiliazation.
4- Measurements (20 Samples).
5- XSHUT Pulled Low again.
Just after the initializing of the VL53L4CD, the current consumption was 4.45uA, then after HW-Standby, I can't get less than 332uA!?

Why this high amount of consumption even if the XSHUT is Pulled Low?
The used board is the Sparkfun board(the LED on the board is removed).
I posted this question inside another topic but I think it's better to be alone(since the sensor is different).
Thank you
Amir