Skip to main content
DM.16
Visitor II
May 1, 2023
Question

VL53L4CX outdoor performance

  • May 1, 2023
  • 2 replies
  • 6978 views

Hi,

I'm trying to use VL53L4CX sensor outdoor as people passing counter. Is there any way to extend outdoor range of the sensor or tune detection parameters? Currently i'm getting around 50-60cm in overcast conditions.

Damjan

This topic has been closed for replies.

2 replies

Zhiyuan.Han
Technical Moderator
May 4, 2023

Hi Damjan

As sun light contain 940nm IR light, which means noise to VL53L4CX sensor, suggest you changing distance mode to short and increase Timing budget. it will help increase maximum detection distance a bit, but will not much.

Br

Zhiyuan.Han

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
John E KVAM
ST Employee
May 10, 2023

If you can afford it the VL53L8CX has almost 3x the optical power of the L4CX. It's better in outdoor lighting.

There is a spec in the L8 datasheet stating it can range to 1.6m in pretty bright light. (I forget the LUX number they used.)

the L8 is also interesting because it is a multi-zone sensor. With it, you can see left/right or up/down motion as someene goes past. It's an easier sensor to turn into people passing sensor. You can tell in which direction they are passing.