VL53L4CX Sensor Measurement Issue – Incorrect Readings Beyond 2 Meters
Hii,
I am writing to seek support regarding an issue I am facing with the VL53L4CX Time-of-Flight sensor. In my current setup, I’m consistently encountering incorrect distance measurements beyond 2 meters, where the sensor tends to report values that are approximately 75-85 cm more than the actual distance.
Details of the Issue:
- Setup: Indoor environment, with stable power supply, targeting a white sheet-covered wall.
- Timing Budget: Set to the maximum value of 200ms.
- Observations: While the sensor occasionally reports the correct distance, more often than not, the values are incorrect, with a significant error margin of 75-85 cm. The status returned is also zero, indicating no error according to the API.
Steps Already Taken:
- Environmental Factors: The sensor is used indoors with no direct sunlight or ambient IR interference.
- Cross-talk Compensation: Using cross-talk compensation function provided in driver.
- Field of View Adjustments: Limited any possible interference from surrounding objects, but the problem persists.
I would greatly appreciate any guidance or suggestions you might have for addressing this issue, or if there are any firmware updates or additional calibration procedures I should follow.
Looking forward to your expert advice.