VL53L4CX-The effect of close, highly reflective objects on SPADs
- March 8, 2024
- 1 reply
- 2845 views
Hi,
I have two questions about the SPAD:
1: How does the L4CX select which part to turn off and which part to turn on when the signal is so large that the SPAD needs to be scaled down? Because i have a Lens installed on the light receiving area, I'm worried if the spad turn off the signal-sufficient part .
2: Is it possible to adjust my SPAD area by ROI? The manual of the L4CX says that this function is not supported, but I found the API function .
Below I would like to explain the problem I'm having:
In order to increase the signal at the far end, I installed a spotlight lens on the light receiving part.
I then noticed that when detecting the appearance and disappearance of white objects in close distance, the data returned by the L4CX was not very stable, with continuous error reporting and data abnormality.
I found that when the anomaly occurred, both the signal and the spad were abnormal, so I suspect it was caused by the spad opening position.
I've uploaded the data from the test, which may help in analysing my problem.
Thanks a lot.