Skip to main content
Associate II
October 3, 2024
Solved

VL53L5CX/8CX LookUp-Table

  • October 3, 2024
  • 1 reply
  • 784 views

Hi,

i know that there are already a few posts on this topic, and i know the VL53L8CX has the same table as the VL53L5CX. But i just wanted to know, if anyboy could post the calculations for the LookUp-Table?

Thanks!

Best answer by John E KVAM

I can't find the spreadsheet where we did the calculations, but it's basically just trigonometry.

There is a discussion of the math in Calculate x,y,z coordinates of each points of the ... - STMicroelectronics Community, but it's really hard to read. 

The light goes out in a pyramid of light 43 degrees on a side. If you are using an 8x8 resolution, then the width of each zone is 5.4 degrees. But we are considering that the distance you get is at the center of each zone. So 2.7 degrees to the right and 2.7 degrees up, would be the center of one of the zones nearest to the mid point. You also get 2.7 degrees left and 2.7 degrees down. 

So if you take a string pointing from the sensor 2.7 degrees right and 2.7 degrees up and at a distance given by the sensor you get a point in space. But that's not a very good coordinate system. 

Some people like polar coordinates - meaning an angle (think 1:30 on your clock) and a radius of some distance and then a height. 

But you can translate that point in space to an X, Y, Z coordinate system as well. But it takes a bit of thinking and book on trigonometry. 

1 reply

John E KVAM
John E KVAMBest answer
ST Employee
October 3, 2024

I can't find the spreadsheet where we did the calculations, but it's basically just trigonometry.

There is a discussion of the math in Calculate x,y,z coordinates of each points of the ... - STMicroelectronics Community, but it's really hard to read. 

The light goes out in a pyramid of light 43 degrees on a side. If you are using an 8x8 resolution, then the width of each zone is 5.4 degrees. But we are considering that the distance you get is at the center of each zone. So 2.7 degrees to the right and 2.7 degrees up, would be the center of one of the zones nearest to the mid point. You also get 2.7 degrees left and 2.7 degrees down. 

So if you take a string pointing from the sensor 2.7 degrees right and 2.7 degrees up and at a distance given by the sensor you get a point in space. But that's not a very good coordinate system. 

Some people like polar coordinates - meaning an angle (think 1:30 on your clock) and a radius of some distance and then a height. 

But you can translate that point in space to an X, Y, Z coordinate system as well. But it takes a bit of thinking and book on trigonometry.