VL53L5CX: Conflicting comments in ULD API and single 4x4 threshold
Greetings - within the "Example_9_detection_thresholds.c" , there a comment (line 164) stating:
"... Please note that the
first one must always be set with a mathematic_operation
VL53L5CX_OPERATION_NONE...."
Yet, within "vl53l5cx_plugin_detection_thresholds.h" it states (line 120):
"...Please note that the first checker MUST always be a OR
operation...."
Base on the example code is working, I assume the first is correct?
Q2 - Single 4x4 threshold: To validate what I'm testing is correct, for single a 4x4 threshold would look something like this:
for (uint8_t i = 0; i < 16; i++) {
thresholds[i].zone_num = i;
thresholds[i].measurement = VL53L5CX_DISTANCE_MM;
thresholds[i].type = VL53L5CX_IN_WINDOW;
thresholds[i].mathematic_operation = VL53L5CX_OPERATION_NONE;
thresholds[i].param_low_thresh = 400;
thresholds[i].param_high_thresh = 800;
}
thresholds[15].zone_num = VL53L5CX_LAST_THRESHOLD | thresholds[15].zone_num;
TIA,
-Terry