VL53L5CX data is never ready
Hello !
I'm working on the VL53L5CX sensor with a Nucleo L432KC.
Using the ST example, and after succeeded the initialization of the VL53L5CX, the sensor's data are never ready. In the following function, the p_dev->temp_buffer[1:4] are all equals to 0 :
uint8_t vl53l5cx_check_data_ready(
VL53L5CX_Configuration *p_dev,
uint8_t *p_isReady)
{
uint8_t status = VL53L5CX_STATUS_OK;
status |= RdMulti(&(p_dev->platform), 0x0, p_dev->temp_buffer, 4);
for (uint8_t i = 0; i < 4; i++)
printf("0x%02X", p_dev->temp_buffer[i]);
printf("\n");
if((p_dev->temp_buffer[0] != p_dev->streamcount)
&& (p_dev->temp_buffer[0] != (uint8_t)255)
&& (p_dev->temp_buffer[1] == (uint8_t)0x5)
&& ((p_dev->temp_buffer[2] & (uint8_t)0x5) == (uint8_t)0x5)
&& ((p_dev->temp_buffer[3] & (uint8_t)0x10) ==(uint8_t)0x10)
)
{
*p_isReady = (uint8_t)1;
p_dev->streamcount = p_dev->temp_buffer[0];
}
else
{
if ((p_dev->temp_buffer[3] & (uint8_t)0x80) != (uint8_t)0)
{
status |= p_dev->temp_buffer[2]; /* Return GO2 error status */
}
*p_isReady = 0;
}
return status;
}
So do you know why this buffer is always equal to 0, and make the sensor never ready ?
Thank you !
Clément Poisson.