Skip to main content
EPARM.1
Visitor II
September 28, 2022
Question

VL53L5CX datasheet, table 17 & 18: definition of typical and minimum values

  • September 28, 2022
  • 1 reply
  • 719 views

Hi,

I need to get distances of objects located between 1.40 m and 2.50 m away from the sensor (cardboard or film-wrapped cardboard) in various light light conditions. 8x8 ranging continuously @ 2Hz.

Some of measured distances (real world) are over the typical and minimum values in table 18, page 20. Does it mean they are not trustable ?

How to interpret terms "typical" and "minimum" for the maximum range capabilities ?

Thanks.

This topic has been closed for replies.

1 reply

Anne BIGOT
Technical Moderator
October 10, 2022

Hello,

What ST guarentees is at least the values of the datasheet. If you are over, it is OK. Your values are trustable.

Typical/minimum are meant for mechanical samples that are issued from the production factory.

Typical samples are the ones which represent the main part of the samples.

Minimum samples are the ones which have mechanical tolerances near the assembly limits.

Regards

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'