VL53L5CX Distances Don't Match Theory - What am I missing?
I am on a robotic forum where we have been studying using this VL53L5CX for robotic vision, mapping and SLAM for the last two months. We are on page 12 of this thread: "<link provided if requested and I'm permitted>"
The problem we have run into concerns the distance readings we're getting out of it. The problem is explained in detail in the second half of this post "<link provided if requested and I'm permitted>" with pictures and previous posts to that thread give detailed output from the sensor.
Since I am new to this forum and can't provide the links, I'll summarize the problem here:
- We have the sensor square-on to a wall 1000 mm away.
- The wall is house-painted white
- The ambient lighting is very low (barely readable)
- Since the FoV angle from corner to corner is ~64 degrees, the corner distances should follow standard Trigonometry theory and be further away than the central pixels.
Theory says, if the center is 1000 mm away, the distance to the center of all four corner pixels should be ~1112 mm away. The sensor is only returning values close to 1018 mm away. IOW, Not anywhere near close to theory. We have tried many different settings for Integration Time (5 to 100 ms) and Sharpness Percent (0 to 99%).
Because it is SO wrong, I feel like I'm missing something fundamental here. Maybe someone here can enlighten me. No one on our forum has seen a problem with our logic and expectations.
Thank you for your time.
VBR,
Inq