VL53L5CX Offset Calibration
Hi,
I noticed that an offset calibration function is missing in the API of the VL53L5CX (like seen before on VL53L1CX). Only the xtalk calibration is available.
Is this because all the VL53L5CXs are individually factory offset-calibrated?
My assumption is also based on the following section of the vl53l5cx_init() function:
/* Get offset NVM data and store them into the offset buffer */
status |= WrMulti(&(p_dev->platform), 0x2fd8,
(uint8_t*)VL53L5CX_GET_NVM_CMD, sizeof(VL53L5CX_GET_NVM_CMD));
status |= _vl53l5cx_poll_for_answer(p_dev, 4, 0,
VL53L5CX_UI_CMD_STATUS, 0xff, 2);
status |= RdMulti(&(p_dev->platform), VL53L5CX_UI_CMD_START,
p_dev->temp_buffer, VL53L5CX_NVM_DATA_SIZE);
(void)memcpy(p_dev->offset_data, p_dev->temp_buffer,
VL53L5CX_OFFSET_BUFFER_SIZE);
status |= _vl53l5cx_send_offset_data(p_dev, VL53L5CX_RESOLUTION_4X4);where offset data are readed from NVM and loaded into the offset buffer.
Offset calibration on host side must be implemented when VL53L5CX is integrated behind a clear plastic glass with low crosstalk component?
Thank you