vl53l5x GO2 error on 8x8 resolution
Hi,
I managed to get the sensor working with firmware VL53L5CX_1.3.11. It works even if I reduce the data load and disable everything except distance.
My problem is, that I do not receive any data if I switch the resolution to 8x8 - the sensor is only delivering data in 4x4 resolution. This happens for all data and for only distance data.
I tried several different chips. The error code is 167 = 0xa7 in check_data_ready (GO2 error status). I got no error before neither when switching the resolution nor when starting ranging.
Thanks