Skip to main content
JGarrettW
Associate II
August 17, 2023
Solved

VL53L8CH Drop in for VL53L8CX

  • August 17, 2023
  • 3 replies
  • 2973 views

I'd like to work with the raw histogram data from the VL53L8CH, which I don't believe the VL53L8CX has. Currently, I don't think that there's an evaluation board for the VL53L8CH, but it says it is "pin-to-pin" compatible with the VL53L8CX. Does this mean that I could remove the VL53L8CX from its evaluation board and drop in the VL53L8CH?

As a side question, I know that the VL53L3CX is not supposed to have accessible raw histogram data, but does if you view the raw serial data after connecting to the evaluation GUI. Is this the same for the VL53L8CX? I was just discussing this with a professor who I believe was helped by @John E KVAM a while ago.

Also, thank you all so much for your help! Forums like this make it so much easier for researchers to get new ideas developed.

This topic has been closed for replies.
Best answer by Zhiyuan.Han

Hi JGarrett

As L8CX and L8CH are sharing the same evaluation board, you don't need to do hardware modification.  

In short, the same L8CX board can be used for both CH and CX evaluation.

Br

Zhiyuan.Han

 

3 replies

Zhiyuan.Han
Zhiyuan.HanBest answer
Technical Moderator
August 22, 2023

Hi JGarrett

As L8CX and L8CH are sharing the same evaluation board, you don't need to do hardware modification.  

In short, the same L8CX board can be used for both CH and CX evaluation.

Br

Zhiyuan.Han

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JGarrettW
JGarrettWAuthor
Associate II
August 23, 2023

Thanks @Zhiyuan.Han. So, I just purchase an L8CH Satel breakout board to connect to the evaluation board? I'm not seeing that available from any of your distributors. How do I evaluate the VL53L8CH? My specific application needs histogram data, so using the VL53L8CX would be harder if I am understanding the differences correctly.

Zhiyuan.Han
Technical Moderator
August 29, 2023

Hi JGarrettW

As you already have L8CX evaluation board, X-NUCLEO-53L8A1, you can connect this board on STM32F401(the white board) for L8CH evaluation.

 

Br

Zhiyuan.Han

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Anne BIGOT
Technical Moderator
September 1, 2023

@JGarrettW 

To evaluate the VL53L8CH, you need for the HW the X-NUCLEO-53L8A1. It has on it a super component covering the VL53L8 series. For the SW, you can download package from this page : STSW-IMG043.

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'