Skip to main content
256
Associate
February 4, 2025
Solved

VL53L8CX at 60 Hz

  • February 4, 2025
  • 3 replies
  • 1070 views

I am trying to run a VL53L8CX sensor at the maximum advertized speed. Originally, following the marketing for this chip, I had thought that this was possible at the full 8x8 sensor resolution, but later learned that that has a maximum speed of 15 Hz (strangely, an associate of mine was able to get it to work closer to 20 Hz, but no faster). We need to have the sensor running at 60 Hz, even if at a reduced resolution, but all examples we can find online are below that 20 Hz threshold. Does anyone have any advice for settings and configurations to bring this sensor to maximum speed? For example, beyond cutting the resolution down by 75%, do we also have to use SPI? Are there any important clock speed values that have to be set to some specific maximums?

For reference, I am running the board with an ESP32 S2 Dev Module board.

Best answer by John E KVAM

You sure can lower the amount of data the sensor sends. 

Have a look at the Platform.h file. 

Make sure Targets is set to 1.

#define VL53L8CX_NB_TARGET_PER_ZONE 1U
(It goes up to 4, but that quadruples the number of targets per zone - and the data returned.)
Uncomment all the ones below that you are not interested in seeing. 
// #define VL53L8CX_DISABLE_AMBIENT_PER_SPAD
// #define VL53L8CX_DISABLE_NB_SPADS_ENABLED
// #define VL53L8CX_DISABLE_NB_TARGET_DETECTED
// #define VL53L8CX_DISABLE_SIGNAL_PER_SPAD
// #define VL53L8CX_DISABLE_RANGE_SIGMA_MM
// #define VL53L8CX_DISABLE_DISTANCE_MM
// #define VL53L8CX_DISABLE_REFLECTANCE_PERCENT
// #define VL53L8CX_DISABLE_TARGET_STATUS
// #define VL53L8CX_DISABLE_MOTION_INDICATOR

You need NB_TARGET_DETECTED, DISTANCE and STATUS.

The rest you can use or not use as you see fit. I recommend Reflectance Percent. It can be useful.

But check:

If  nb_target_detected>1 AND target_status ==0 then you have a valid target at distance_mm.

- john

3 replies

John E KVAM
ST Employee
February 5, 2025

Sorry for the slow post (technical issues.)

The VL53L8CX affectionately known as the L8 can do 15 frames per second in 8x8 mode and 60 frames per second in 4x4 mode. 

The trick is to insure your I2C can handle the data. Depending on which options you choose in the Platform.H file, you can generate some 2000 bytes per frame. And that adds up.

Yes, you can push the sensor to 20 frames. But be a little careful here. Less integration time means a less accurate answer - and you cannot 'see' quite as far. (The sensor does not get as many photon strikes with a shorter integration time.) But if you don't need to see out to the full 4 meters and you have a reasonably bright target, it will work just fine.

We got the results in the datasheet by running at 15 frames, so we set that as the 'practical' max. 

But give it a try. 

And you might be able to drive the 4x4 to 80 frames, but that's a lot of testing on your part to ensure your answer is good enough for you.

- joh

256
256Author
Associate
February 7, 2025

I think I understand. Thank you. We have been able to get three 4x4 sensors operating just under 60 Hz now, thanks to the VL53L8CX being capable of 1 MHz trasmission over I2C (in case anyone in the future needs it, here's the command, to be put after DEV_I2C.begin(): DEV_I2C.setClock(1000000)).

I do have one more question though, regarding speed. In our testing, we have found that, when the sensor returns NA for the majority of its measurements, it ends up being a bit faster than when the measurements are within range. I believe this may be due to the limited processing power on the board to accomplish the calculations it is doing for each measurement (as covered in this question). Becuase of this, I would like to deactivate as much of the on-board calculations (for the L8) as possible, so I can choose to do them myself on my more powerful computer or other board. 

To do this, I've been looking at the vl53l8cx_api.c file, and having been trying to parse all of the different options available for disabling functions contained within it:

VL53L8CX_USE_RAW_FORMAT, VL53L8CX_DISABLE_MOTION_INDICATOR, VL53L8CX_DISABLE_TARGET_STATUS, and VL53L8CX_DISABLE_DISTANCE_MM, for example.

Do you know of a good resource out there I could use to understand what each of these (not including the ones with obvious names, of course) are doing? And if deactivating them (by defining them in the platform_config_default.h file) will allow the VL53L8CX to operate a little bit faster?

 

John E KVAM
John E KVAMBest answer
ST Employee
February 10, 2025

You sure can lower the amount of data the sensor sends. 

Have a look at the Platform.h file. 

Make sure Targets is set to 1.

#define VL53L8CX_NB_TARGET_PER_ZONE 1U
(It goes up to 4, but that quadruples the number of targets per zone - and the data returned.)
Uncomment all the ones below that you are not interested in seeing. 
// #define VL53L8CX_DISABLE_AMBIENT_PER_SPAD
// #define VL53L8CX_DISABLE_NB_SPADS_ENABLED
// #define VL53L8CX_DISABLE_NB_TARGET_DETECTED
// #define VL53L8CX_DISABLE_SIGNAL_PER_SPAD
// #define VL53L8CX_DISABLE_RANGE_SIGMA_MM
// #define VL53L8CX_DISABLE_DISTANCE_MM
// #define VL53L8CX_DISABLE_REFLECTANCE_PERCENT
// #define VL53L8CX_DISABLE_TARGET_STATUS
// #define VL53L8CX_DISABLE_MOTION_INDICATOR

You need NB_TARGET_DETECTED, DISTANCE and STATUS.

The rest you can use or not use as you see fit. I recommend Reflectance Percent. It can be useful.

But check:

If  nb_target_detected>1 AND target_status ==0 then you have a valid target at distance_mm.

- john