vl6180 liquid measure
I need to measure the level of a transparent liquid of small depth (5-20mm). I try vl6180 or vl6180X. The sensor is located at a height of 30-40mm from the bottom. The sensor does not see the liquid. It shows the distance to the bottom. If you gradually pour liquid into a container, the measured distance does not change. Only if the liquid level reaches 40-60mm does it show that there is something in the tank, but it is wrong (if the distance to the liquid is 30mm, it shows 40-50). I can not use the float. Is it possible to solve this problem?