VL6180 proximity detection logic output mode
Hi,
I would like to know if we can configure GPIO0 or GPIO1 as a logic output mode. In datasheet, we can configure in INT mode. But we need to clear the flag each time we have a value. So we have a wrong value during the clearing.
I would like to configure the sensor for exemple 40cm detection, and have "1" when we detect somthing, and "0" when not without clearing or something else. Is that possible ?