Why are the ranging results of different VL6180X-Sensors so extremely deviating?
Hi, I've testet four Time-of-Flight-Sensors of the type VL6180. The results were all different, for a distance of eg 30mm I got 23mm (Sensor1), 21mm (Sensor2), 16mm (Sensor3) and 32mm (Sensor4). The measurements all took place under the same conditions. I'm very interested in the reason of the results.
(Could it be, that the soldering of the pins and the causing higher temperature are the reason for that or is it because of the manufacting tolerance?)