Skip to main content
Levan
Associate II
March 12, 2024
Question

Antenna diversity implementation on SPIRIT1 transciever

  • March 12, 2024
  • 0 replies
  • 779 views

Hi all,

I have a question regarding the SPIRIT1 RF transceiver. According to Section 9.1, it features Antenna diversity functionality, allowing the transceiver to monitor signal strength in antennas and utilize the best one available.

Levan_0-1710229970845.png

My query is whether this function is directly implemented on SPIRIT1 or if it necessitates a host MCU where all the logic will be housed to control diversity functions.

If its implemented on SPIRIT1, is it function via the available four GPIO pins?

Are there any specific requirements for RF switches to enable this function?

Moreover, is it feasible to employ four antennas, or does this functionality exclusively support two antennas?

Thank you

This topic has been closed for replies.