Best Bus for connecting several STM32's
Hello guys, I am a new B and have started the cours of leaning coding and CubeMX, but I would really use some of your enlightenment!
I've been playing around with a couple of 3D printer boards using Marlin Firmware to drive my Pick and Place Machine for a while now. But Marlin is not to good at supporting more than one nozzle and 3D printer boards are not really interesting for dedicated PnP machines using Open PnP software! So I have decided to build my own eco system using ST32H 's! The only downside is my knowledge in CubeMX and coding language, neither the less I am a very fast learner, so I came her to get some guidance for my project!
Unlike the all in one 3D printing motion controller boards, I plan my system modules like!
1 -The "Master Module" with USB in from the computer, SD Card for firmware updates, Ethernet, I2C, SPI and CAN FD! (Maybe using a STM32H745)
2 -X & Y Axis Stepper Motor Driver Module, receiving real time commands from the "Master Module" via the best Bus! (Maybe using a STM32H743)
3 -Z's Axis Stepper Motor Driver Module, receiving real time commands from the "Master Module" via the best Bus! (Maybe using a STM32H743)
4 -C's Axis Stepper Motor Driver Module, receiving real time commands from the "Master Module" via the best Bus! (Maybe using a STM32H743)
5 -Analog In Module for vacuum sensors (Maybe using a STM32H743)
6 -Digital Out Module for Actuators (Maybe using a STM32H743)
ETC...
I think by now you get the idea which leads to my 3 questions:
First "Are the 2 STM32's of my choice up to the task, if yes fine if not what choice would be better?"
And second "What would be the best Bus to use in such configuration, knowing that a minimum of wires are recommended for connection
to the whole gantry and head to reduce the moving weight?"
A good start is better than a quick start in my case, so I would really use your enlightening advices for my project while I get familiar with coding
and with this amazing tool CubeMX!!!!
Thanks Much