Skip to main content
SK.10
Associate
September 20, 2020
Question

BLUE-NRG-232 DC-DC converter modes

  • September 20, 2020
  • 4 replies
  • 1353 views

We are using BLUENRG-232 in one of our low cost designs. On page 138 of the datasheet, we can see two DC-DC converter configs. For cost savings, we would like to go with non-active DC-DC converter config. However, there isn't much info available about the power consumption or performance impact. I would like to have a deeper understanding of both active and non-active DC-DC converter modes.

This topic has been closed for replies.

4 replies

Winfred LU
ST Employee
September 25, 2020

On page 146, Table 212.

There are 2 parts for the table : when DCDC converter active and when DCDC converter not active.

RX and TX power will be higher in the case DCDC converter is not active.

SK.10
SK.10Author
Associate
September 25, 2020

Thanks for the response. I have a question regarding the RF section. We are using BLUENRG-232 in conjunction with BALF-NRG-02D3. While it says that the impedance of both the devices are matched, there is no exact info of how much show the differential impedance of the traces be, Is it 100 ohms differential impedance?

Winfred LU
ST Employee
September 28, 2020

It will be 50 ohm.

SK.10
SK.10Author
Associate
September 28, 2020

So I don't need to route them as a differential pair? The RF0 and RF1 traces? Just route them as single ended 50 ohm?

Winfred LU
ST Employee
September 29, 2020

Please refer to BlueNRG-2 datasheet, table 217.

0693W000004I2j0QAC.png

SK.10
SK.10Author
Associate
September 30, 2020

I have seen this one. But not sure what trace impedance to use since the impedance mentioned in the table is a complex impedance.