BlueNRG 2
I am working with BlueNRG 2, and Tile both... I'm working in BlueNRG-1_2 DK 3.2.3. In the xx\BlueNRG-1_2 DK 3.2.3\Firmware\BLE_Examples\BLE_SerialPort\BlueNRG-2 folder, there is Server bin and hex files which work great. However, when I go to the C:\ST\BlueNRG-1_2 DK 3.2.3\Project\BLE_Examples\BLE_SerialPort\EWARM\BlueNRG-2 folder, there is only source code for the Client. I need the Server source/project files that were used to build the bin and hex.