BlueNRG-2
Hi,
Please help if possible.
I have an automotive electronic board which has a BlueNRG-2 device on it and it runs Yocto Linux on its main processor which is connected to the Ble chip via UART interface. I have loaded the the BlueNRG-2 device with DTM firmware hence I can control the chip using hcitool by sending HCI commands over the uart. I have managed to put the device into connectable advertisement or Beacon modes so I can connect to it from my phone using "nRF Connect" or "BLE Scanner" apps. However, from the moment the connection between the phone and BlueNRG-2 device is made, it takes about 30 seconds and the connection drops and I cant connect to it anymore unless I repeat the whole steps again. why the connection drops? I am doing the same thing with STEVAL-ID00BV2 board and noting goes wrong, the connection stays alive until I disconnect it myself.
thanks for help.
Roosbeh