Skip to main content
Steven1
Associate
December 15, 2020
Question

BlueNRG-2N firmware not working on X-NUCLEO-BNRG2A1

  • December 15, 2020
  • 0 replies
  • 488 views

Hello,

I have the SampleApp running with the BlueNRG-2 firmware on the X-NUCLEO-BNRG2A1. When I reflash the X-NUCLEO-BNRG2A1 with the BlueNRG-2N firmware the SampleApp stops working. It runs again when I switch back to the original firmware.

BlueNRG-2 firmware used:

DTM_SPI.hex

BlueNRG-2N firmware used:

BlueNRG_2N_FW_V3_2_0.bin

Am I missing some configuration steps or something else completely?

Best regards,

Steven

    This topic has been closed for replies.