Skip to main content
Senior
January 28, 2024
Solved

BlueNRG-LP I2C1 and I2C2 coexistence

  • January 28, 2024
  • 6 replies
  • 2716 views

hello community,

I´m using PB10/PB11 as I2C1 and PB6/PB7 as I2C2.

Danny0007_0-1706436538253.png

I2C1 works correctly.

But I2C2 not, after reset on PB6 and PB7 I just get some messy signals as below, It seems the I2C2 is not initialized with succcess.

Danny0007_1-1706436961888.png

Actually the both I2C are initialized in the same way:

Here is the pin definition for both I2C

//sensor1
#define BSP_I2C                                   I2C1
#define BSP_I2C_CLK_ENABLE()                      LL_APB1_EnableClock(LL_APB1_PERIPH_I2C1)
#define BSP_I2C_CLK_DISABLE()                     LL_APB1_DisableClock(LL_APB1_PERIPH_I2C1)

#define BSP_I2C_DATA_PIN                          LL_GPIO_PIN_10
#define BSP_I2C_DATA_GPIO_PORT                    GPIOB
#define BSP_I2C_DATA_GPIO_PULL                    LL_GPIO_PULL_NO
#define BSP_I2C_DATA_GPIO_AF()                    LL_GPIO_SetAFPin_8_15(GPIOB, LL_GPIO_PIN_10, LL_GPIO_AF_2)
#define BSP_I2C_DATA_GPIO_CLK_ENABLE()            LL_AHB_EnableClock(LL_AHB_PERIPH_GPIOB)
#define BSP_I2C_DATA_GPIO_CLK_DISABLE()           LL_AHB_DisableClock(LL_AHB_PERIPH_GPIOB)

#define BSP_I2C_CLK_PIN                           LL_GPIO_PIN_11
#define BSP_I2C_CLK_GPIO_PORT                     GPIOB
#define BSP_I2C_CLK_GPIO_PULL                     LL_GPIO_PULL_NO
#define BSP_I2C_CLK_GPIO_AF()                     LL_GPIO_SetAFPin_8_15(GPIOB, LL_GPIO_PIN_11, LL_GPIO_AF_2)
#define BSP_I2C_CLK_GPIO_CLK_ENABLE()             LL_AHB_EnableClock(LL_AHB_PERIPH_GPIOB)
#define BSP_I2C_CLK_GPIO_CLK_DISABLE()            LL_AHB_DisableClock(LL_AHB_PERIPH_GPIOB)

//sensor2
#define BSP_I2C2                                   I2C2
#define BSP_I2C2_CLK_ENABLE()                      LL_APB1_EnableClock(LL_APB1_PERIPH_I2C2)
#define BSP_I2C2_CLK_DISABLE()                     LL_APB1_DisableClock(LL_APB1_PERIPH_I2C2)

#define BSP_I2C2_DATA_PIN                          LL_GPIO_PIN_7
#define BSP_I2C2_DATA_GPIO_PORT                    GPIOB
#define BSP_I2C2_DATA_GPIO_PULL                    LL_GPIO_PULL_NO
#define BSP_I2C2_DATA_GPIO_AF()                    LL_GPIO_SetAFPin_0_7(GPIOB, LL_GPIO_PIN_7, LL_GPIO_AF_0)
#define BSP_I2C2_DATA_GPIO_CLK_ENABLE()            LL_AHB_EnableClock(LL_AHB_PERIPH_GPIOB)
#define BSP_I2C2_DATA_GPIO_CLK_DISABLE()           LL_AHB_DisableClock(LL_AHB_PERIPH_GPIOB)

#define BSP_I2C2_CLK_PIN                           LL_GPIO_PIN_6
#define BSP_I2C2_CLK_GPIO_PORT                     GPIOB
#define BSP_I2C2_CLK_GPIO_PULL                     LL_GPIO_PULL_NO
#define BSP_I2C2_CLK_GPIO_AF()                     LL_GPIO_SetAFPin_0_7(GPIOB, LL_GPIO_PIN_6, LL_GPIO_AF_0)
#define BSP_I2C2_CLK_GPIO_CLK_ENABLE()             LL_AHB_EnableClock(LL_AHB_PERIPH_GPIOB)
#define BSP_I2C2_CLK_GPIO_CLK_DISABLE()            LL_AHB_DisableClock(LL_AHB_PERIPH_GPIOB)

Here is the init function for both I2C

//sensor1

void BSP_I2C_Init(void)
{
  /* Initialize the GPIOs associated to the I2C port */
  BSP_I2C_DATA_GPIO_CLK_ENABLE();
  LL_GPIO_SetPinMode(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_MODE_ALTERNATE);
  LL_GPIO_SetPinSpeed(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_SPEED_FREQ_HIGH);
  LL_GPIO_SetPinOutputType(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_OUTPUT_OPENDRAIN);
  LL_GPIO_SetPinPull(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, BSP_I2C_DATA_GPIO_PULL);
  BSP_I2C_DATA_GPIO_AF();

  BSP_I2C_CLK_GPIO_CLK_ENABLE();
  LL_GPIO_SetPinMode(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_MODE_ALTERNATE);
  LL_GPIO_SetPinSpeed(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_SPEED_FREQ_HIGH);
  LL_GPIO_SetPinOutputType(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_OUTPUT_OPENDRAIN);
  LL_GPIO_SetPinPull(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, BSP_I2C_CLK_GPIO_PULL);
  BSP_I2C_CLK_GPIO_AF();

  /* Initialize the I2C clock */
  BSP_I2C_CLK_ENABLE();

  LL_I2C_Disable(BSP_I2C);

  /* Configure the SDA setup, hold time and the SCL high, low period
   * For Fast-mode 400 kHz, PRESC | 0h | SCLDEL | SDADEL | SCLH | SCLL
   *                          1h  | 0h |    3h  |   2h   |  03h |  09h
   */
  LL_I2C_SetTiming(BSP_I2C, 0x10320309);

  /* Enable Clock stretching */
  LL_I2C_EnableClockStretching(BSP_I2C);

  /* Enable Peripheral in I2C mode */
  LL_I2C_SetMode(BSP_I2C, LL_I2C_MODE_I2C);

  /* Enable the I2C peripheral */
  LL_I2C_Enable(BSP_I2C);

  /* Enable I2C transfer complete/error interrupts:
   *  - Enable Receive Interrupt
   *  - Enable Not acknowledge received interrupt
   *  - Enable Error interrupts
   *  - Enable Stop interrupt
   */
//  LL_I2C_EnableIT_TX(BSP_I2C);
//  LL_I2C_EnableIT_RX(BSP_I2C);
//  LL_I2C_EnableIT_TC(BSP_I2C);
//  LL_I2C_EnableIT_NACK(BSP_I2C);
//  LL_I2C_EnableIT_ERR(BSP_I2C);
//  LL_I2C_EnableIT_STOP(BSP_I2C);
}
 
//sensor2
void BSP_I2C2_Init(void)
{
  /* Initialize the GPIOs associated to the I2C port */
  BSP_I2C2_DATA_GPIO_CLK_ENABLE();
  LL_GPIO_SetPinMode(BSP_I2C2_DATA_GPIO_PORT, BSP_I2C2_DATA_PIN, LL_GPIO_MODE_ALTERNATE);
  LL_GPIO_SetPinSpeed(BSP_I2C2_DATA_GPIO_PORT, BSP_I2C2_DATA_PIN, LL_GPIO_SPEED_FREQ_HIGH);
  LL_GPIO_SetPinOutputType(BSP_I2C2_DATA_GPIO_PORT, BSP_I2C2_DATA_PIN, LL_GPIO_OUTPUT_OPENDRAIN);
  LL_GPIO_SetPinPull(BSP_I2C2_DATA_GPIO_PORT, BSP_I2C2_DATA_PIN, BSP_I2C2_DATA_GPIO_PULL);
  BSP_I2C2_DATA_GPIO_AF();
  BSP_I2C2_CLK_GPIO_CLK_ENABLE();
  LL_GPIO_SetPinMode(BSP_I2C2_CLK_GPIO_PORT, BSP_I2C2_CLK_PIN, LL_GPIO_MODE_ALTERNATE);
  LL_GPIO_SetPinSpeed(BSP_I2C2_CLK_GPIO_PORT, BSP_I2C2_CLK_PIN, LL_GPIO_SPEED_FREQ_HIGH);
  LL_GPIO_SetPinOutputType(BSP_I2C2_CLK_GPIO_PORT, BSP_I2C2_CLK_PIN, LL_GPIO_OUTPUT_OPENDRAIN);
  LL_GPIO_SetPinPull(BSP_I2C2_CLK_GPIO_PORT, BSP_I2C2_CLK_PIN, BSP_I2C2_CLK_GPIO_PULL);
  BSP_I2C2_CLK_GPIO_AF();
  /* Initialize the I2C clock */
  BSP_I2C2_CLK_ENABLE();

  LL_I2C_Disable(BSP_I2C2);
  /* Configure the SDA setup, hold time and the SCL high, low period
   * For Fast-mode 400 kHz, PRESC | 0h | SCLDEL | SDADEL | SCLH | SCLL
   *                          1h  | 0h |    3h  |   2h   |  03h |  09h
   */
  LL_I2C_SetTiming(BSP_I2C2, 0x10320309);
  /* Enable Clock stretching */
  LL_I2C_EnableClockStretching(BSP_I2C2);
  /* Enable Peripheral in I2C mode */
  LL_I2C_SetMode(BSP_I2C2, LL_I2C_MODE_I2C);
  /* Enable the I2C peripheral */
  LL_I2C_Enable(BSP_I2C2);
  /* Enable I2C transfer complete/error interrupts:
   *  - Enable Receive Interrupt
   *  - Enable Not acknowledge received interrupt
   *  - Enable Error interrupts
   *  - Enable Stop interrupt
   */
//  LL_I2C_EnableIT_TX(BSP_I2C);
//  LL_I2C_EnableIT_RX(BSP_I2C);
//  LL_I2C_EnableIT_TC(BSP_I2C);
//  LL_I2C_EnableIT_NACK(BSP_I2C);
//  LL_I2C_EnableIT_ERR(BSP_I2C);
//  LL_I2C_EnableIT_STOP(BSP_I2C);
}
 
***********************************************************************
any idea?
thanks in advance.

Danny

This topic has been closed for replies.
Best answer by Danny0007

ladies and gentlemen,

I measured the power pin and put my board under microscope and find out it was a power issue. 
Now clock signal is normal.

btw: does CubeIDE support BlueNRG-LP?  I mean BlueNRG-LP as main cpu.

6 replies

Danny0007Author
Senior
January 31, 2024

Let´s make this question more simple, only I2C2(PB6/7) is not working

this is the pin definition:

Danny0007_0-1706737096197.png

this is my init function:

Danny0007_1-1706737138479.png

 

 

Danny0007Author
Senior
January 31, 2024

even the clock signal is not correct:

Danny0007_0-1706738416610.png

Danny0007_1-1706738441649.png

 

Rene Lenerve
ST Employee
February 1, 2024

Hi Danny0007,

Here are some points to check as both I²C are initialized identically:

- Check I²C registers are correctly set in the MCU just before first communication (need debug)

- Check I2C2EN = 1 and I2C2RST = 0 (need debug)

- Check pull-up resistors are correctly soldered on I²C bus lines SCL and SDA (externally to MCU, keep GPIO no pull up option set in MCU)

Could you get a capture of the first byte sent (device select) for I²C1 and I²C2.

Kind Regards.

Danny0007Author
Senior
February 1, 2024

Hi Rene,

thanks for the reply!

I found this in the document RM0479 page 106:

Danny0007_0-1706822111029.png

Does it mean that the PB6/7 as I2C2 only support either standard mode or FM+? Fast mode at these pins are not supported. Because in my init function for I2C2 I just copied the timing setting from I2C1(PB10/11), which supports fast mode.

Danny0007_1-1706822318829.png

I do find this tools from ST and try to reproduce this settings, then change it to standard mode or FM+

Danny0007_2-1706822479044.png

If this is the reason, could you teach me how to set the parameters in the table correctly and firstly reproduce the timing setting for fastmode? 

 

 

Rene Lenerve
ST Employee
February 2, 2024

Hi Danny0007,

The Fast mode+ allows the I²C to operate at 1Mbit/s, compared to the standard mode and the fast mode speed which are 100kbit/s and 400kbit/s respectively. Both I²C1 and I²C2 support all these modes, but for FM+ on dedicated pins.

ReneLenerve_0-1706864424048.png

 

I2C I/Os supports 20 mA output current drive for fast-mode plus operation.
This is enabled by setting the driving capability control bits for SCL and SDA
in Section 8.2.3 I2C Fast-Mode Plus pin capability control register (I2C_FMP_CTRL).

 

 

The timings from I²C1 are based on a 16MHz I²C source clock and are given in the Reference Manual in the table 58

ReneLenerve_1-1706865086462.png

The clock for I²C1 and I²C2 is fixed and set to 16MHz (picture from RCC section, green line)

ReneLenerve_2-1706866305251.png

The PCLK is used for registers only (blue line, Figure 83 in Reference Manual).

So if you want to change the i²C mode, refer to table 58.

May I point you to an ST Tool (if you don't already know it) that will allow you to configure your MCU and which will generate code to initialize peripherals that you need (STM32CubeMX):

https://www.st.com/en/development-tools/stm32cubemx.html

This may help you to see if you missed something in your settings. This tool is also available in STM32CubeIDE if you use it for your developments.

Hope this can help you.

Kind Regards.

 
 

 

 

Danny0007Author
Senior
February 2, 2024

Hi @Rene Lenerve 

I tested standard mode, the PB6/7 signal looks similar as before, not working.

and I cannot find chip BlueNRG-LP in cubeMX and and cubeIDE

 

Danny0007AuthorBest answer
Senior
February 4, 2024

ladies and gentlemen,

I measured the power pin and put my board under microscope and find out it was a power issue. 
Now clock signal is normal.

btw: does CubeIDE support BlueNRG-LP?  I mean BlueNRG-LP as main cpu.

Rene Lenerve
ST Employee
February 5, 2024

Hi Danny0007,

Great that it's working now.

For BlueNRG-LP and CubeMX, sorry for the confusion, this MCU is not available in cubeMX I was merely thinking about the timing computation for the I²C, but as the peripheral clock is fixed for I²C, there is no need to recompute timings, those provided in the Reference Manual are sufficient.

Hope this can help you

Kind Regards.