[BlueNRG-MS] Can't connect to gatt server with Android device
Hello,
I created a BLE peripheral using a BlueNRG-MS chip. I can connect on this peripheral using a BlueNRG-M2 (using BlueNRG GUI) and read the services.
However, it does not work when I try to connect with an android device (I use "BLE Scanner" app, Bluepixel Technologies). Here are the steps :
- I run my app on BlueNRG-MS (peripheral) ✔�?
- I start BLE Scanner on android ✔�?
- I see my BlueNRG-MS peripheral on the android app, then I click on "CONNECT" ✔�?
- The BlueNRG-MS seems to accept the connexion since it returns an HCI_LE_META_EVENT the following data :
- Event Code 0x13 (HCI_LE_META_EVENT)
- Subevent_Code 0x01 (HCI_LE_CONNECTION_COMPLETE)
- Status 0x00 (Success) ✔�?
5. The android app seems to try to connect during 10s, then it says "connection failed" �?��?
I tested different android apps and the result is the same. I guess there are some parameters incompatible with android bluetooth ?
The android app (BLE Scanner) is working with BlueNRG-M2 controlled with BluenRG GUI.
Thanks for reading,
Best regards,
Valentin