BlueNRG: Not notified when attribute is written
I have modified the BlueNRG sensor demo adding a new characteristic to turn on/off a LED. I want to be notified when the client (the smartphone) sends data so I can check the written value to change the LED status accordinly.
I have tried many options but I am not being notified for writes, only for reads.
This is the characteristic added (just bellow de humidity characteristic):
COPY_LED_CHAR_UUID(uuid);
ret = aci_gatt_add_char(envSensServHandle,
UUID_TYPE_128,
uuid,
2,
CHAR_PROP_WRITE | CHAR_PROP_WRITE_WITHOUT_RESP,
ATTR_PERMISSION_NONE,
GATT_NOTIFY_WRITE_REQ_AND_WAIT_FOR_APPL_RESP | GATT_NOTIFY_ATTRIBUTE_WRITE,
16,
0,
&ledCharHandle);
if (ret != BLE_STATUS_SUCCESS) goto fail;
charFormat.format = FORMAT_UINT16;
charFormat.exp = -1;
charFormat.unit = UNIT_UNITLESS;
charFormat.name_space = 0;
charFormat.desc = 0;
uuid16 = CHAR_FORMAT_DESC_UUID;
ret = aci_gatt_add_char_desc(envSensServHandle,
ledCharHandle,
UUID_TYPE_16,
(uint8_t *)&uuid16,
7,
7,
(void *)&charFormat,
ATTR_PERMISSION_NONE,
ATTR_PERMISSION_NONE,
ATTR_ACCESS_WRITE_REQ_ONLY,
16,
FALSE,
&descHandle);
if (ret != BLE_STATUS_SUCCESS) goto fail;The return value is BLE_STATUS_SUCCESS
Then, in the user_notify callback, I add the EVT_BLUE_GATT_WRITE_PERMIT_REQ event but it is never called.
case EVT_VENDOR:
{
evt_blue_aci *blue_evt = (void*)event_pckt->data;
switch(blue_evt->ecode){
case EVT_BLUE_GATT_READ_PERMIT_REQ:
{
evt_gatt_read_permit_req *pr = (void*)blue_evt->data;
Read_Request_CB(pr->attr_handle);
break;
}
// ADDED THE WRITE REQUEST NOTIFICATION
case EVT_BLUE_GATT_WRITE_PERMIT_REQ:
{
evt_gatt_write_permit_req *pr = (void *)blue_evt->data;
Write_Request_CB(pr);
break;
}
}
}Am I missing something? do I need to do anything else in order to get the write notifications? (read notifications work perfectly)
I have been stuck with this for a long time, any help will be appreciated!
Thanks