Configuration of the X-Nucleo-BNRG2A1 board connected to a Nucleo L476RG board.
Hello everyone,
I bought an X-Nucleo-BNRG2AI board for a project I need to do using Bluetooth. I currently work with the Nucleo L476RG and got the Bluetooth expansion to attach to it.
At the moment, I’m facing some difficulties getting it to work. All the material I find is a few years old, and in some forums, it’s mentioned that much of it is no longer valid.
Right now, I just want to transmit something via Bluetooth, but I can’t make it work. I’m looking into firmware updates or something similar, but nothing I’ve tried has worked. I’ve followed all the processes described in AN5651, but there’s always some kind of error. I found a forum suggesting the STM32CubeProgrammer, but I also encounter errors when trying to connect with the X-Nucleo-BNRG2AI. If anyone could help me with any updated procedures or something along those lines, I’d appreciate it.
BR,
Felipe.