Connect to TLV493D-A1B6 over I2C
Hi folks
I am currently trying to communicate with the TLV493D-A1B6 3D hall sensor. As board, I'm using the NUCLEO-F103RB. To make sure I didn't mess up any connections or anything else, I verified my setup with an ADS1015 adc which I can read out over I2C. Unfortunately, I am not able to find a valid address whilst sweeping through all possible addresses. I always get "HAL_ERROR" after using the following routine. With my other I2C device, I get 3 valid addresses.
for(i=1; i<255; i++)
{
ret = HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(i<<1), 3, 5);
if (ret != HAL_OK) /* No ACK Received At That Address */
{
HAL_UART_Transmit(&huart1, Space, sizeof(Space), 10000);
}
else if(ret == HAL_OK)
{
sprintf(Buffer, "0x%X", i);
HAL_UART_Transmit(&huart1, Buffer, sizeof(Buffer), 10000);
}
}For further information, any data sheets are available here: https://www.infineon.com/cms/en/product/sensor/magnetic-sensors/magnetic-position-sensors/3d-magnetics/tlv493d-a1b6/
Thanks a lot for your help and best regards