Difficulties in connecting to BLE devices
Hello,
I am using a BlueNRG-2 acting as a central to connect with multiple BLE devices, these devices can connect and disconnect multiple times.
I am using up to 6 simultaneous connections to different devices, after some successful attempts I keep getting errors from the ST API during the connection stage, usually at the pair/bonding stage.
The errors are either:
- BLE_STATUS_NOT_ALLOWED (0x46): no further information is available and I cannot understand why is this operation not allowed when calling 'aci_gap_send_pairing_req()'?
- BLE_STATUS_DEV_IN_BLACKLIST (0x59): how can I access and handle this blacklist, information on this is nonexistent, can I remove devices from the blacklist or prevent them from being stuck there?
When a connection fails the system seems to enter a loop and cannot recover.
Most commonly, what happens is that when there is an error, the initial connection is successful, but the process fails when negotiating at the encryption step (I am using default encryption with fixed pin).
I think this question might be similar to another posted to this forum but with no response so far, titled:
"STM32WB pairing error with mixed bonded/nonbonded devices
Thanks in advance.