Skip to main content
Associate II
August 28, 2024
Solved

Does RFID Transponder M24LR04E-RMN6T/2 work with Mifare Desfire

  • August 28, 2024
  • 3 replies
  • 2288 views

Hi.

Please can someone tell me whether Part No: M24LR04E-RMN6T/2 (RFID Transponder) is able to communicate with MiFare Desfire ?

Application will be a custom designed PCB to be used as part of Prepaid payment system

 

CW1_0-1724828828979.png

 

 

Thanks

Best answer by Peter BENSCH

Of course! Unlike proprietary solutions from competitors, STMicroelectronics fully complies with the NFC standard. Depending on the desired range and security, however, it may make sense to use the more modern NFC Forum Type 5 standard instead of Type 4 tags, for which the ST25DVxxK  (ISO15693) are ideally suited.

3 replies

Peter BENSCH
Technical Moderator
August 28, 2024

Welcome @CW1, to the community!

First of all a note: M24LR04 are already on NRND (Not Recommended for New Design).

Furthermore, MIFARE® DESFire® complies with ISO14443, M24LR04 to ISO15693 and is therefore not suitable.

Regards
/Peter

CW1Author
Associate II
August 28, 2024

Hi Peter,

Thank you for the prompt response.

I assume that M24LR04 has been replaced with a newer version. Am I correct ? If so, can you give me the new Part number.

Thanks

CW1Author
Associate II
August 28, 2024

Also, does the newer version comply with ISO14443 ?

Peter BENSCH
Technical Moderator
August 28, 2024

NFC tags comply with either ISO14443 or ISO15693, not both.

Yes, M24LRxx has been replaced by ST25DVxx, but it is also ISO15693. The only Dynamic Tags still available with ISO14443 are M24SR02, M24SR04, M24SR16 and M24SR64.

However, you should note that MIFARE Desfire uses a proprietary protocol, the details of which are probably only communicated by NXP under NDA. STMicroelectronics cannot help you with this and cannot provide any software for MIFARE Desfire.

Good luck!
/Peter

CW1Author
Associate II
August 28, 2024

Understood.

Does ST offer it's own protocol for ST25DVxx or otherwise is there some form of open source protocol that is compatible with these chips ?

Peter BENSCH
Technical Moderator
August 28, 2024

STMicroelectronics cannot have or offer its own protocol for MIFARE Desfire, as it uses a proprietary protocol as mentioned above. Nothing can exist as open source either, because the proprietary protocol mentioned is closed source and therefore completely contradicts the idea of open source.