Skip to main content
MSyai.1
Associate
January 11, 2023
Solved

Hello, I'm very new to STM32 and LCD RGB. Currently, I bought the LCD TFT AFY480272A0-4.3INTH. It says that the interface uses a 24-bit parallel RGB. Can I drive it using the NUCLEO-F767ZI? And, how do I connect the flexible cable to the Nucleo pin?

  • January 11, 2023
  • 1 reply
  • 2060 views

..

This topic has been closed for replies.

1 reply

MM..1
MM..1Best answer
Chief III
January 11, 2023
MSyai.1
MSyai.1Author
Associate
January 12, 2023

Thanks, I'll order it soon. But I'm still confused about how to set the brightness on the Nucleo. The backlight has two pins, an anode and a cathode. The forward voltage of the backlight is 18V.0693W00000Y81KnQAJ.png0693W00000Y81MAQAZ.png