Skip to main content
merivel
Associate
June 5, 2023
Question

Hi, in sw package BlueNRG-2 “over-the-air�? (OTA) firmware upgrade what happened in case : 1 - power failure during upgrade? 2 - lost of BLE during update? in configuration OTA service manager framework

  • June 5, 2023
  • 3 replies
  • 1042 views

..

This topic has been closed for replies.

3 replies

merivel
merivelAuthor
Associate
June 5, 2023

.

Winfred LU
ST Employee
June 6, 2023

Refer to:

AN4869: The BlueNRG-1, BlueNRG-2 BLE OTA (over-the-air) firmware upgrade

With the OTA service manager framework, the firmware will be corrupted. The user has to restart the OTA upgrade procedure.

With the reset manager and the higher/lower application approach, the new firmware is corrupted too. But, the old firmware application can still work, since only (approximately) half of the flash memory was to be upgraded.

merivel
merivelAuthor
Associate
June 6, 2023

When BLE communication is lost, reestablishing the OTA upgrade procedure happens automatically after a timeout or requires a manual reset?