How does STUSB4500 handle a USB Power Delivery 3.1 Source PDO?
I've written an STUSB4500-based MCU application that displays the voltage and current options available from a USB-C adapter, and allows you to select one.
New chargers that support USB Power Delivery 3.1 can offer Source PDOs above 20V. For example, the Apple 140W charger offers a Source PDO of 28V 5A.
Do I need to filter out a PDO greater than 20V before using it to set up a Sink PDO on the STUSB4500, or is this done automatically by the STUSB4500? I'm concerned that a 28V VBUS would damage the STUSB4500 and surrounding circuitry.