How exactly to adjust output power on S2LP?
What is the simplest way to set the power amplifier?
Unfortunately the APIs require involvement with the PA ramps and index configurations.
void S2LPRadioSetPALeveldBm(uint8_t cIndex, int32_t lPowerdBm)
void S2LPRadioSetMaxPALevel(SFunctionalState xNewState)
I'm trying a simple low level configuration:
write( PA_POWER0, 0x00 ) // PA_POWER0 disable all features and select PA_LEVEL_1 slot
write( PA_POWER1, 0x01 ) // PA_POWER1 = 29-2*dBm dBm=14
or
write( PA_POWER1, 0x5B ) // PA_POWER1 = 29-2*dBm dBm=-31
That guess is based on the SigFox S2-LP driver and the data sheet. It doesn't work. Does this suggest the API to turn down the power in the SigFox drivers doesn't work? Or am I missing something about how these don't apply to CW mode or there's missing charge pump or SMPS voltage configurations?
https://github.com/sigfox-tech-radio/sigfox-ep-rf-api-st-s2lp/blob/417f31d94d4a95266c61f6b75f1cfa34a7fffe7e/src/manuf/s2lp_rf_api.c#L661