I made an acquisition board with STM32WB55rgv6. I want to save ads1299 sampling data to SD card by FATFS(via spi). But my write speed is only 1KB. Here are the measures I have tried: ①Improve SPI clock ②Replace faster SD card ③Mybuffer is 51200B
Although every time I write in a single block instead of multiple blocks, and I only use SPI, not DMA. But the write speed is too low, only 1KB. I've browsed through many measures, but they still haven't saved me. I used stm32cubeide to develop this project,
project opening address C:\Desktop\STM32Cube_FW_WB_V1.1.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\FatFs\FatFs_uSD_Standalone\SW4STM32