MODBUS RTU reading problems
I have a problem with modbus-rtu communication in my stm project.
The STM32F446RE is connected to a MAX485 board by UART1 to RO-DI pin and by a GPIO pin to RE-DE.
A typical instruction (variable:INSTRUCTION.array_instruction) is something like 01 06 26 04 00 57 + CRC16 (variable:cksum16).
Where:
01 slave address
06 write single instruction
26 04 my instruction
00 57 instruction value
xx xx CRC1
Here my programm:
HAL_GPIO_WritePin(MODBUS_DE_RE_GPIO_Port, MODBUS_DE_RE_Pin, GPIO_PIN_SET); //MAX485 write mode
HAL_Delay(DELAY_FOR_MODBUS);
HAL_UART_Transmit(&huart1,(uint8_t*)&INSTRUCTION.array_instruction,6,1000);
HAL_UART_Transmit(&huart1,(uint8_t*)&cksum16,2,1000);
HAL_Delay(DELAY_FOR_MODBUS);And all works great for all kind of write instructions (0x06).
The problems come with read function.
After sending a request (01 03 00 00 00 01 +crc 84 0A) I read my port
HAL_Delay(DELAY_FOR_MODBUS);
HAL_GPIO_WritePin(MODBUS_DE_RE_GPIO_Port, MODBUS_DE_RE_Pin, GPIO_PIN_RESET); //MAX 485 read mode
HAL_Delay(DELAY_FOR_MODBUS);
HAL_UART_Receive(&huart1,(uint8_t*)given_response.array_response,sizeof(response),3000);
HAL_Delay(DELAY_FOR_MODBUS);But "given_response.array_response" is always 00 00 00 00 00 00 00 and not 01 03 xx xx xx +crc16 xx xx
I tried with greater DELAY_FOR_MODBUS value (now =10 for 19200 baud serial) and longer timeout, with no results.
Thanks a lot,
Mario