Port X-CUBE-BLE2 code to BLUENRG2-M2SA
Hi,
We are developing a project with BLE connectivity, and we are leaning on using BLUENRG-M2SA as a network coprocessor, with a STM32L476 MCU as the host processor.
We have been experimenting with X-NUCLEO-BNRG2A1 ( that has BLUENRG-M2SP on it ), and have ported example code ('Central' and 'VirtualCOM') from STM32CubeIDE ( X-CUBE-BLE2.3 SW package) with success. Also, we have used RF-Flasher utility to flash firmware (BLUENRG-M2SP_DTM_SPI.hex from BlueNRG-M2SA_M2SP_DTM_Stack_v2.1c) directly to M2SP, also with success.
Finally, we tried unsoldering and replacing M2SP with M2SA on BNRG2A1 development board. However, despite being able to flash BLUENRG-M2SA_DTM_SPI.hex correctly, and while being able to recognize and send commands successfully with BLUENRG-GUI, the X-CUBE-BLE2 examples (particularly 'Central') doesn't work. In fact, it fails on initization.
Is there any change in X-CUBE-BLE2 SW that needs to be done, so that projects that run on M2SP also run in M2SA ?
I changed the #define's in bluenrg1_devConfig.c according to the DT0137 paper, but didn't make any difference